VT-RNSII-ptH (benchtop)

Features

VT-RNSII-ptH portable model new generation.

Designed for off-line inspection, the VT-RNSII-ptH is an ideal solution for smaller manufacturers running low volume or prototyping assembly lines. The inspection algorithms used in the VT-RNSII-ptH are identical to the fully automated in-line machine, the VT-RNSII.

The system uses Omron’s patented RGB ‘Color Highlight’ system which has proven so successful. This lighting system illuminates the target from all angles and in all directions in a 360 degrees dome (dome illumination).  The advantage of dome illumination is that it enables stable performance of inspection regardless of component placement directions or other angle designs.  In high-density placement applications, the reflective luminosity of the solder surface is diminished by the shadows of adjacent components.

VT-RNS2-PTH presents very high capability for post solder inspection, whether it is post-reflow or post-wave inspection. A wide range of algorithms allows the machine to perform top quality inspection, still in line with the highest demand today.

With EzTS (EasyTeach software), a program can be created in minutes with very fast library creation and extra fine tuning capability. This is a perfect tool for new programmers as well as experienced programmers.

VT-RNS2-PTH benefited of the all the improvement made by OMRON with colour image processing since the launch of the first AOI machine using colour image processing in the mid-80’s.

Still today, VT-RNS2-PTH is compatible with the latest software technology with WINDOWS7 operating system and the possibility to connect it to an MES system.

  • Patented 3 ‘Color highlight’ technology
  • High resolution inspection using 3CCD camera
  • True colour image processing 
  • EasyTeach (EzTS) for fast and automatic program creation  à Read more
  • User-friendly Repair/Verification Station software (RVS)  à Read more
  • Statistical analysis and reporting tool (Line Status Reporter, LSR)  à Read more
  • Character verification
  • Lead-free enabled 
  • Full compatibility of the programs with the RNS2 in-line machine.
  • VT-RNS2 can also be used for post-placement inspection or 2D solder paste inspection.
  • Available for Medium Size PCB (333x255mm) or Large Size PCB (550x650mm)
  • WINDOWS7

EasyTeach (EzTS)

The EasyTeach (EzTS) Software can be used “off-line” for creation and modification of inspection programs. It can also be use “in-line” for program tuning during inspection without stopping or slowing down the production line. Working in this way the machine is never a bottleneck, even if some tuning is being made or not during inspection mode. The optimization of the programs on the off-line programming station during inspection ensures implementation time and the uploading of programs from the inspection results is as fast as possible. Recommended feature on all VT-RNS2 machines for both in line and desktop models.  

  • Easy Library Creation
  • Very Fast program Creation (PCB 100x100, 50cpts, 20cpt types) = 20min from Scratch +Lib
  • Automatic component creation using populated and bare board and “program creator wizard”
  • Preset of colour parameters and criteria using first few boards. à Ready for production before fine tuning.
  • Possibility to compare images of false rejects, OK or real defects from previous/next boards, same/other location, same type etc…

Line Status Reporter (LSR)

Line Status Reporter LSR for VT RNS acquires, collects and displays in a graph form the inspection and repair results from the RNS machine:

  • Defect reports with defect images for each faulty component.
  • Displays graphs for PCB, component type, component variation, component name, defect name analysis.
  • LSR is recommended on VT RNS2 machines for both in-line and desktop models.
  • Very Simple and user friendly.

Repair/Verification Station Software (RVS)

RVS verification Station software is used to verify very easily the results from the AOI machine. This software is very user friendly and the display of very clear colour images of the defects can only help the operator for the best and easiest judgment possible. Using this RVS software, there is no need of magnifying equipment as the image provided is enough to see the fault very clearly. This software can be installed in-line straight after the AOI in the case of 2D Solder paste inspection, post placement inspection or post solder inspection. This way, the faulty PCB results are displayed automatically by the Checking Software after the inspection is complete. RVS-I Inline Checking Station is recommended for Paste and Placement inspection applications. After Solder inspection, RVS-D Batch Checking Station Software can be used and the results are loaded after scanning the PCB-ID of the faulty PCB.

Have a question?

We are ready to help.

Contact us

Distributor Lookup

Our distributors are positioned to give you outstanding technical support and service.

Find a distrubutor near you

Subscribe to product updates

Newsletters about product innovations, solutions and services, directly in your inbox.

Thank you for subscribing to Omron's eNews. You will shortly receive an e-mail from us. This e-mail contains a link which activates your email newsletter subscription. This method is used due to legal issues and to make certain that no-one can abuse your e-mail address.

We are experiencing technical difficulties. Your form submission has not been successful. Please accept our apologies and try again later. Details: [details]

Download

Events and fairs

See our systems in use and consult our experts.

View upcoming events